Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Xplained-Slide3

A microcontroller is needed to interpret the data from the sensor and then do something with that data. Examples of actions to be taken are to present the data to the user, deploy the airbag or to control an object in a game. The microcontroller often uses data fusion in order to give meaningful feedback to the user application. This implies taking data from more than one sensor type. The algorithm commonly used in a digital compass takes data from both the magnetometer and the acceleometer to tell where the user is heading.

PTM פורסם ב: