Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PowerStor Supercapacitors Slide 14

Individual supercapacitors are typically limited to a maximum operating voltage of 2.5V. As many applications require higher voltages, supercapacitors are commonly configured in series to increase the working voltage. When doing this it is important to ensure that the individual voltage of any single supercapacitor does not exceed its maximum rating as this could result in electrolyte decomposition, gas generation, ESR increase and reduced lifetime.

PTM פורסם ב: