Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PowerStor Supercapacitors Slide 18

Inflow current is a combination of charge current and leakage current, leakage current is a parasitic element that is modeled as a resistor in parallel with the capacitor. This parallel resistance presents a constant load to the supply and causes the capacitor to self discharge when the supply voltage is removed. Due to supercapacitor construction it takes a very long time for full charge to be achieved, even after 100 hours it is still possible to measure a few micro Amps of charge current. As a result supercapacitors have to be charged for over 100 hours to get a good indication of leakage current or self discharged characteristics.

PTM פורסם ב: