Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PowerStor Supercapacitors Slide 8

From the charts shown it can be seen that both capacitance and ESR vary with temperature. Above 20 degrees Celsius the capacitance increases and ESR decreases giving a greater design margin. Below 20 degrees Celsius the capacitance decreases and ESR increases. Allowances need to be made for these changes in order to ensure the selected capacitor operates correctly over the required temperature range.

PTM פורסם ב: