Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PowerStor Supercapacitors Slide 5

Using the four basic parameters and the equation i = C . dv/dt, where “i” is the discharge current, C is the capacitance, dv is the change in voltage and dt is the duration of the discharge, we can calculate the minimum required capacitance assuming zero voltage drop across the ESR. For example a system has a nominal voltage of 2.5 Volts and a drop out voltage of 2.0 Volts. The system must continue to operate for 5 seconds after a mains fail and has an average current demand of 0.5 Amps. In this case the minimum allowable capacitance will be 5 Farad.

PTM פורסם ב: