Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PowerStor Supercapacitors Slide 20

From the table of leakage current per Farad it can be seen that leakage current varies with temperature, the above plot shows how the leakage current of a 0.47F, 5V part varies as the temperature is cycled from 85 °C down to 25 °C and back up again with measurements taken at 40 °C and 70 °C. This clearly shows that, although leakage current increases with temperature it is a process that is reversed as the temperature decreases.

PTM פורסם ב: