Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Comparison Between Silicon vs. Silicon Carbide

The main difference between silicon and silicon carbide devices is that silicon carbide has a higher dielectric breakdown electric field at 2.8 MV/cm compared to only 0.3 MV/cm of regular silicon. Because of this, power devices built with silicon carbide can be made shorter to just 1/10th the length, which then further reduces ON-resistance and ultimately conduction loss. In addition, silicon carbide devices have much lower reverse recovery charge, resulting in lower switching losses. In fact, up to 74% lower switching losses can be seen with SiC FETs compared to IGBT + FRD solutions. Silicon carbide devices provide high-voltage switching voltage conversion with lower losses versus their silicon counterparts.

PTM פורסם ב: