Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Trends in DC Charging Stations

The ever-increasing demand for EVs to drive longer distances with a single charge has steadily increased EV battery capacity over time. At the same time, the trend towards higher power DC fast-charge stations has also increased. DC fast-charging stations contain multiple power supply units (PSU), as shown here in the diagram. Each PSU must provide more than 40 kW of power in order to supply a total of more than 350 kW. The circuit topology trend is to use a 3-phase Vienna rectifier along with silicon carbide devices to provide a high-efficiency solution with better thermal management capability.

PTM פורסם ב: