Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Types of Electric Vehicle Charging

There are two types of electric vehicle (EV) charging. AC charging takes power directly from the power grid and connects to an onboard charger mounted in the EV itself. The onboard charger converts the AC voltage into DC voltage which is then used by the battery management system (BMS) to charge and control the battery. DC charging first converts AC power from the grid to DC voltage via an off-board charger in a DC charger station. The DC voltage is then directly provided to the battery management system within the EV, allowing optimization of the off-board charger at the DC charging station to scale up and deliver much higher power to the BMS.

PTM פורסם ב: