Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide11

The operating temperature in an ‘under the hood’ environment ranges from -55°C to 150°C.  With a moving vehicle the liquid can sway when turning or hitting a bump in the road. If the liquid is near the low level sensing point, the sensor may energize creating an alert of a fault condition. During vehicle swaying the alert may come on and then go off repeatedly. A wide hysteresis built into the sensor will prevent this. Once the sensor is activated, it must remain on until brake fluid has been added. Furthermore, like all plug-in electrical connections, the contacts can oxidize or corrode interrupting the electrical connection particularly in the ‘under the hood’ environment. So the sensor must include the ability to let the on-board computer know that the sensor is properly connected to the electrical system.

PTM פורסם ב: