Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide12

The hermetically sealed reed sensor is the best choice and satisfies all the brake fluid sensing requirements. In this case, a float with an imbedded magnet is placed within the brake fluid tank in an area where it can ride up and down with the brake fluid. The reed switch is directly mounted to a printed circuit board which also houses a high kilo-ohm resistor with two rugged terminals. These components are further housed in a plastic sealed package that locks in place in the lower external section of the brake fluid tank. The reed sensor is plugged into a sealed automotive electrical connector allowing connection to the vehicle electrical system.

PTM פורסם ב: