Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide13

When the brake fluid level with the float is low enough, the magnet within the float will activate the reed switch. The reed sensor will then turn on an indicator light on the dashboard alerting the driver of the low fluid level. It also turns off and alerts the operator the ABS braking system is turned off.

PTM פורסם ב: