Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide28

If the liquid is near the low level sensing point, the sensor may energize creating an alert of the fault condition. During vehicle swaying the alert may come on and then go off repeatedly. A wide hysteresis built into the sensor will prevent this. Once the sensor is activated, it must remain on until washer fluid has been added. The specific gravity can vary depending upon the level of alcohol within the fluid. The specific gravity can alter the level of the position of the float within the liquid giving rise to different turn-on and turn-off points.

PTM פורסם ב: