Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide26

The level sensor will need to operate 100% of the time in a wet, dirty, ‘under the hood’ environment. Mechanical sensors have been used in the past, but not being hermetically sealed, they have encountered faulty operation due to contamination affecting their operation. The sensor needs to be capable of operating as low as -55°C and as high as 150°C, and must be sealed to handle the rough environment.

PTM פורסם ב: