Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide3

The reed switch is a small electromechanical switching device that has two ferromagnetic leads encased in a hermetically sealed glass cylinder. Ferromagnetic materials are materials that become magnetized when they enter or are influenced by a magnetic field. Iron, nickel, and cobalt are the most common ferromagnetic materials. The leads are internally aligned and separated by a gap. The reed switch can be as small as 4mm and as large as 50mm long.

PTM פורסם ב: