Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide22

Because of the criticality of sensing the movement of the brake pedal, it is vital that the dirty, wet environment have no effect on reliability of the sensor operation. Choosing a hermetically sealed reed sensor that is further packaged in a rugged plastic housing is essential for fault free operation. Also, the reed sensor can remotely sense distances greater than one inch. This is important because the brake pedal can have significant movement to it. The sensing distance must be capable of maintaining its closure from the initial movement of the brake pedal to the end of its movement. In this manner, the brake lights stay on and the cruise control remains off.

PTM פורסם ב: