Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
IGBT and SLLIMM IPM Slide 3

This slide shows how to build a part number using ST’s new part number nomenclature for the Trench Gate Field Stop IGBTs. As in the past, ST IGBT part numbers begin with the STG prefix, followed by an alphabetic character denoting package type. The following two numeric characters denote the maximum continuous current rating at 100°C, followed by an alphabetic character denoting the IGBT technology, which indicates operational speed range and its tradeoffs between conduction losses and switching energy losses. The next alphabetic character indicates special features if they are included. One or two alphabetic characters in the next spot indicate whether or not a Freewheeling diode is co-packaged with the IGBT die, and whether it is a very-fast recovery, ultra-fast recovery, or low forward voltage drop diode. The next character being an F denotes that the device is a Trench Gate Field Stop technology IGBT, and the subsequent numeric character indicates the generation. If there is no numeric character the device is generation one, generation two when indicated by a number 2, etc.

PTM פורסם ב: