Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
IGBT and SLLIMM IPM Slide 30

The breakdown of the Gen 2 SLLIMM part number nomenclature is shown on this slide. All SLLIMM IPM module part numbers begin with STGI, where the G indicates it is an IGBT based device and the I indicates a SLLIMM IPM module. The fifth alpha character relates specifically to Gen 2 devices, indicating whether or not the part has a DBC thermal interface substrate or is a full molded epoxy package. The sixth and seventh numeric characters indicate the maximum continuous current at 25°C. The eighth and ninth alpha characters indicate the technology speed of the IGBTs employed. The tenth and eleventh numeric characters indicate the IGBT breakdown voltage, divided by ten. The next three alpha characters indicate the type of temperature sensing or thermistor used, or if it has one at all. The last character indicates whether or not the package is a short or long lead package.

PTM פורסם ב: