Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 14

A pair of L6202 used with the L6506 or L297 implements the complete interface from the microcontroller to the motor with very few external components, mainly the current sense resistor, resistor divider to set the reference voltage and the bootstrap capacitors. When using the L6203 in this configuration motor currents in excess of 3 amps can be supplied. As technology has improved so has the level of integration achieved in the motor driver ICs.

PTM פורסם ב: