Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 30

When the left transistor turns off, the voltage on it’s drain will fly back to the clamp voltage and be clamped by the diode/zener clamp. The voltage on the collector of the right transistor will go down at the same time so that the voltage across the two halves of the coil is the same. Since the clamp voltage is more than twice the supply voltage the voltage at the collector of the right transistor will go negative. In Darlington arrays, like the ULN2000 series, taking one of the collector output pins below the chip ground can cause substrate injection which can make the device operate improperly or may even lead to catastrophic failure in some devices. Such Darlington arrays that are not specifically designed to drive steppers are not recommended for this application.

PTM פורסם ב: