Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 2

There are many type of motors used for various applications today. In general they can be divided into two classes: self commutated motors and externally commutated motors. Universal motors and brushed DC motors are the only truly self commutating motors although an induction motor that is connected directly to the mains, single or three phase, requires no commutation to run at constant speed. Motors like steppers, Brushless DC (BLDC), switched reluctance and induction motors driven by variable frequency drives all require external electronics to provide the commutation for the motor. Of these motors, steppers are probably the easiest to drive and that makes them attractive for low cost small power applications.

PTM פורסם ב: