Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 5

The basic block diagram for a bipolar stepper motor driver is shown here. Three main blocks are required for the driver. First, the timing and phase generation to generate the steps. This is generally done with a microcontroller or a microcontroller in conjunction with decoding logic. Next, is the current control. This is typically implemented as a PWM current control. Finally, there is the power driver, which for a stepper, is a dual H-Bridge configuration. For the integrated drivers in that range below 3 Amps and less than 50 Volts we can partition the bridge and the current control in a couple of different ways.

PTM פורסם ב: