Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 28

For unipolar stepper motors the drive configuration is simply 4 transistors to ground. These are grouped in pairs with each pair driving the ends of a single coil that has its center tap connected to a supply voltage. In addition to the transistors we need to add a clamping circuit to clamp the inductive fly back. The zener in the clamp circuit may be connected to ground as shown in the slide, or may be connected back to Vs either configuration is acceptable. The second will have a lower dissipation in the zener.

PTM פורסם ב: