Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 16

The basic device in the family is the L6205. As you see in the block diagram the device implements a dual H-bridge with the gate drive and protection functions. A charge pump that uses external capacitors and diodes provides the gate drive voltage for the upper power MOS transistors. With 4 outputs, implementing the charge pump is a better choice than having the individual bootstrap capacitors like the L6202. Notice that the output of the over current detection circuit is connected to the Enable input of the IC. By putting a simple RC circuit on the enable input the part implements an over current protection that will cause the device to start chopping and limit the current to the peak set by the internal threshold. The over current detection senses the current flowing through the upper MOS transistor using a non dissipative sensing technique. By sensing this current the output can be protected against shorts across the load or shorts to ground.

PTM פורסם ב: