Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 19

The 4th device in the family adds the translator to generate the phase signals. The translator block takes the clock input and generates the phase information based on the direction and control inputs. Like the L297 the device can operate in either full step or half step modes, selected by the control input. Functionally this device replaces two L6202 devices plus the L297 and maintains the same interface to the microcontroller. However, since both bridges are in one package the dissipation is twice the dissipation of the L6202. The current capability of the PowerSPIN family of devices about 1 and a half to 1 and three quarters amps when using the Power SO package mounted on an FR4 board using an optimized layout with a center ground plane.

PTM פורסם ב: