Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 19

With the L6470/74, an SPI interface is all that is required, simplyfing the system from the software and  hardware point of view. Also, if the user has a platform with one motor and then needs to make an evolution with various motors, they can probably keep the same microcontrollers. The MCU is not heavily loaded as the decay timing calculations are performed in the L6470 and L6474.

PTM פורסם ב: