Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 32

In summary, until recently the design of a stepper motor was a fairly complex task. Thanks to the EasySPIN and dSPIN, this is task is greatly simplified. At this time no competitor has similar features, and ST EasySPIN and dSPIN are state of the art stepper motor drivers. In current mode control, the decay is automatically managed and the microstepping can contain up to sixteen microsteps. In voltage mode control, only offered by STMicroelectronics, a true 128 microsteps is achievable. In addition, the speed profile can be generated, plus the STMicroelectronics solution decreases the number of components. All this combines to make the design of high performance stepper motor easy.

PTM פורסם ב: