Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 24

This slide shows the weaknesses of the current mode compared to the voltage mode. In current mode control, when proceeding from one level to another one, it will go as fast as possible to the next one. That can cause some mechanical vibrations, particularly at low speed. At the same time the average current is lower than the target current as a decay is performed as soon as the current is equal to the target current. Therefore the positioning is less accurate and there are some torque ripples. And as the switching frequency is not constant, it is noisy at low speed.

PTM פורסם ב: