Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 22

The block diagram of the L6470 is shown on this slide; it is very similar to the L6474. They both operate from 8 to 45 V, and are offered in HTSSOP and Power SO packages offering high thermal dissipation. The key difference is in the core of the device, using different logic to manage the voltage mode and generate positioning and speed profile.

PTM פורסם ב: