Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 27

This slide shows that with no BEMF compensation, the voltage in the coil would be quickly close to zero, and hence no current would go through the coil and therefore no torque. The motor would stall. Thanks to the BEMF compensation, the current is stable and the torque remains constant. The BEMF value is linear vs. the speed, the L6470 increases the applied voltage linearly vs. the speed in order to come up with a constant current.

PTM פורסם ב: