Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 23

Shown on this slide are the key differences between the voltage mode and current mode. The standard method is the current mode. The EasySPIN uses this mode and brings great improvements to this method. At this time ST is the only one making the voltage mode control.  In current mode, a current is applied to the coil creating a feedback loop which monitors the current. This is a closed loop: when the current is too low, it is increased; when the current is too high, it is decreased with a decay. In the voltage mode, it is completely different because it is an open loop and the current is not monitored. The system applies a voltage to a motor and to the phase. Knowing the specifications of the system (BEMF, resistance and inductance of the motor) the current going through the coils is known. As the torque depends on the current, the idea to control the system with voltage instead of the current can look unusual, but actually brings advantages.

PTM פורסם ב: