Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 9

When the current is stable, due to a chopping technique, the circuit will increase and decrease the energy/current in the coil at a high frequency. Each time the current decreases, it also applies a decay. Depending on the current level and the amplitude from one step to the next, all the timings will be different, explaining the complexity in the design of a stepper motor.

PTM פורסם ב: