Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 26

As explained previously, the challenge in current mode control is the management of the decay timing. Hence, the L6474 has registers to configure this timing. In voltage mode control, as a fixed frequency PWM is applied, the decay is automatic. But as the current depends on the voltage that is applied, the BEMF must be compensated. As the BEMF is a voltage created by the spin of the motor, the total voltage seen by the motor is the voltage applied minus BEMF. The BEMF must be compensated to remove its effects, the device has registers provided to program this compensation.

PTM פורסם ב: