Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 13

In order to avoid entering in an endless loop of ON and OFF, the channels are not turned on simultaneously, but one by one. This allows the system to restart smoothly after a shut down due to an over temperature incident. In other words, an IPS turns on the channels one by one, with a delay of around 100 ms. Hence, step by step, the total current increases smoothly, minimizing the probability of a new over temperature event.

PTM פורסם ב: