Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 28

The VN808 is an 8 channel IPS that can be used to decrease the RDSON too. As a single channel is 160 mOhm, putting the 8 channels in parallel do not bring any improvement versus the 4 channels of the VNI4140. The VN808 is the previous generation versus of the VNI4140 which is the new generation.

PTM פורסם ב: