Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 24

The L6370 is manufactured with Multipower BCD technology and has features that the VIPower technology products do not have. These include: programmable current limit, open ground in ON state and programmable ON delay to drive a capacitive load. The L6370, unlike most of the portfolio that has a current max of 1 A per channel, has a current of 2.5 A per channel.

PTM פורסם ב: