Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 23

This is a comparison between the VNI4140 (new generation) and the VN340 (previous generation). Going to the new generation allows to dissipate less heat (and hence, lose less energy). As heat is often a major constraint in applications using IPS, A lower RDSON allows to decrease the power to dissipate by 42%. This low RDSON on 4 channels is manufactured thanks to the VIPower technology. This technology allows a mono-die solution, even for 4 or 8 channels, increasing the reliability which is an important parameter in industrial applications.

PTM פורסם ב: