Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 6

Shown here are the protection features that can be integrated. An IPS is a MOS with a lot of additional protections and diagnostics. One of the major protections is the short circuit and over-current protection. Remember that the load is between the Vout and the ground. If this pin is short-circuited, the IPS limits the current and the board is not destroyed. There is also the loss of ground protection, so if the wire is cut between the ground and the load, there is open load detection. The over-temperature protection is not just a simple shutdown, but also a management of multiple over temperature events. The fast demagnetization allows safe removal of the energy from a coil and of course these products are designed to meet stringent ESD requirements.

PTM פורסם ב: