Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 22

The VNI4140 is a 4 channel IPS that comes in two flavors. They have all the protection features, the only difference is in the current: The VNI4140 is for 0.7 A with a typical current limit of 1 A. The VNI4140K-32 is for 1 A with a typical current limit of 1.5 A. Like the VNI4120, the RDSON is 80 milliohm and has similar protections.

PTM פורסם ב: