Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 29

The VNI8200 is the new generation and has a 110 mOhm RDSON per channel, so brings a 30% improvement versus the VN808. The purpose of a multi channel IPS, however, is not to only decrease the RDSON by putting the outputs in parallel. The main purpose is to drive several loads in a small space and hence decrease the cost of the final application. The VNI8200 integrates the traditional safety features of an IPS, like current limitation, junction and case over-temperature shutdown. It also integrates an optional SPI. The pin SEL1 allows to program the chip in SPI bus or parallel bus. A parallel bus is faster to turn on and off a channel, but the main advantage of the SPI is the cost saving for the optocouplers, as applications requiring an IPS often need isolation.

PTM פורסם ב: