Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide10

Channel configuration is defined using the ANT serial message protocol. A network key must be defined and sent as the start of the channel set-up, as well as a channel ID of 32 bits, made up of the device ID, device type and transmission type. This ID is the basis of device association. The device ID is a sixteen bit field that is often the variable used to distinguish a device within the network. The device type is used in ANT+, the interoperable application extension, to narrow search variables by pre-defining which device class is transmitting. Transmission type is mostly used to define certain transmission characteristics. In a private network application transmission type offers another unique eight bits of ID. Power output levels are also defined at this stage using the message protocol.

PTM פורסם ב: