Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide27

Acknowledged messages are valuable for links that require assurance of receipt, such as a control application. The slave automatically responds to the sending master that the message had the been received. Though the slave to master acknowledged message uses slightly more power, it is much more reliable over a variety of use cases. Caution must be observed to avoid incorrect state machine transitions. It is recommended not to use a master initiated acknowledged transmission where there is a potential of multiple slaves receiving the signal, the slave can be confused as to which node should respond. As an example, a bike power meter may be transmitting to a watch and a bike computer with both displaying the readings. If an acknowledged message was sent, the watch may respond when the computer is the intended responder.

PTM פורסם ב: