Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide26

Broadcast messages are for connections that do not need assurance of the delivery of the message. Sensors such as temperature, humidity, HR, etc., use this method. The diagram on this slide illustrates two ways that broadcast can be used. Master to slave shows the master sending a packet transmission on its assigned frequency and at its configured message rate (the red block) and then opening a receive window to listen for other transmitters in the time slot. Should there be traffic detected in the receive window, on the next message the master will slightly adjust the transmission period to avoid the noise. The slave to master portion shows that the receiver can also broadcast back to the master. In the case of  a slave that has a message to go back to the master it would use the broadcast data transfer and the master’s receive channel would hear that message and react to it.

PTM פורסם ב: