Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide16

Using the variety of ANT channel options allows the developer to make simple to complex network structures with a variety of data transfer methods that suit the use case challenges they face. Remember that each ANT connection is independently defined and is comprised of one master and one or more slaves. ANT has pre-defined some multi-node configurations to be used as building blocks for more complex structures.

PTM פורסם ב: