Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide32

While ANT is very robust and not normally bothered by other RF signals at times a stationary signal from an 802.11 source of sufficient signal strength and bandwidth may cause an unacceptable packet loss. An ANT channel established using the frequency agility option will sense the loss in quality and move to another pre-configured frequency. The default frequencies are chosen to best avoid WiFi center channels. Acknowledged messages are used to monitor master node service degradation and missed packets on the slave. Frequency agility differs from frequency hopping in that agility only moves when there is low service available. This reduces channel management overhead dramatically.

PTM פורסם ב: