Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide28

ANT offers a burst transfer mode which is ideal for efficiently transferring bulk data at significantly faster rates. Burst messaging is based upon multiple packet, fully acknowledged, message strings. In the string of packet delivery each packet is held in the buffer until the previous packet has been acknowledged. Packet order is also added to the messaging making it easier to reassemble jumbled or restarted packet strings. Burst channels are automated via the protocol. Burst packet size is configurable and ANT will inform the host at the end of the predetermined length of packets. For the only instance in the ANT protocol, failure to receive an ACK from the burst slave will result in an automatic packet resend. This resend will happen up to five times if necessary. The ANT host MCU will be notified on the fifth failure and is expected to take action. The burst train will go into the next period if required. Strong adherence to MCU flow control is required. The asynchronous baud rate is a minimum of 19,200 kbps. The ANT burst transfer mode is optimized and more efficient than synchronous communication data rates.

PTM פורסם ב: