Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide18

The star topology is the next most common ANT network type and is the basis of the most popular sport applications. The display is the slave and the body worn or bike sensors act as independent masters each with their own separate channel set up. The current maximum number of spikes to the star is eight. This is dependent upon the silicon/module choice the user makes. ANT provides the channel scheduling internally so the developer need not worry over collisions between the channels. Pairing of the devices will be discussed in subsequent slides.

PTM פורסם ב: