Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide3

The Open Systems Interconnection model (OSI model) was a product of the Open Systems Interconnection effort at the International Organization for Standardization. It is a way of sub-dividing a communications system into smaller parts called layers. Similar communication functions are grouped into logical layers. A layer provides services to its upper layer while receiving services from the layer below. On each layer, an instance provides service to the instances at the layer above and requests service from the layer below. An ANT engine completes the first four layers of the industry standard leaving application specific layers to the discretion of the developer. This level of integration allows for less network protocol work and more time for the application itself.

PTM פורסם ב: