Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide30

It is possible to have applications that just broadcast data to all slaves, such as access control which alerts the system to new entrants into a building or space. One by one messages are handled easily using this method. For example, in a retail outlet a system could update all prices overnight one at a time. The challenge is assigning slave IDs, an auto shared application is available to allow an ad hoc sensor addition to a polling network.

PTM פורסם ב: