Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide15

By using the RX window during transmit ANT has created a listen before speak scheme so ANT nodes can coexist with a large number of other ANT nodes, or avoid RF noise if necessary. The embedded ANT protocol automatically manages the receive window and maneuvers the open channels away from each other. Up to three hundred nodes can coexists in a 1Hz message rate network. The RX window at transmit time is also used for back channel communication which allows the slave to respond to the master if it has something to say without establishing a new channel.

PTM פורסם ב: